1862534_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1862534_en-US

1862534_en-US

S32DS can't install freertos for S32K344

Hi everyone,

What I saw a post just now is the same as my subject. when I install the offline installation package, I also found I can't install freertos, reporting one or more required tiems could not be found. image as follows:

Hanoch_0-1715258273379.png

it show that I had installed the software., nstallation details as follows: 

Hanoch_2-1715258347550.png

but I can't create new freertos project from k3 example, images as follows:

Hanoch_3-1715258447401.png

how do I install successfully?




Re: S32DS can't install freertos for S32K344

Thanks, it's done!

Re: S32DS can't install freertos for S32K344

Hi @Hanoch 

The FreeRTOS version 2.0.3 was developed for S32DS v3.4 using S32K3 Real-Time Drivers AUTOSAR 4.4 Version 2.0.3. According to the provided information, you are using S32DS v3.5 and RTD v3.0.0; the FreeRTOS version compatible with this SW is the 3.1.0 (SW32K3_FreeRTOS_10.5.1_3.1.0_D2304).


B.R.

VaneB

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 03:11 PM
Updated by: