1861452_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1861452_en-US

1861452_en-US

RTE Real Time Driver

Hi There,

I need some informations about Real Time Enviroment (RTE) SchM_.c, present in S32k RTDs.

In particular,  I noticed that, instead of a  simple "enable interrupt/disable interrupt" -critical section approach, a more complex one is used:

in particular:  SchM_Enter___EXCLUSIVE_AREA_() and SchM_Exit___EXCLUSIVE_AREA_()  methods are implemented (where is the driver name and is an incrementing number

1) could you explain me the ratio under this implementation ? How have I use these functions in my code  ? Why the suddivision for and for

2) If I use this in application, which / ones shall I use? shall I check the implemented ones, in the RTD, before choosing one?,

Best Regards.

Fabio

Re: RTE Real Time Driver

Hello,

NXP provides stubs for AUTOSAR SchM integration. If you are targeting AUTOSAROS, these will need to be replaced by the BSW integrator.

These numbers do not have a meaning other than indicating which register/variable accesses are being protected - See the Integration Manual for the respective module:

bryan_brauchler_0-1715174869879.png

In the most simple case, this can simply disable/enable interrupts. See the Baremetal implementation. In the FreeRTOS case, these map to taskENTER_CRITICAL() and taskEXIT_CRITICAL() but this will be updated in the future as this is not sufficient for critical sections in interrupt context.

Best,

Bryan

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 03:13 PM
更新者: