1861215_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1861215_en-US

1861215_en-US

PN7642 jlink error

Hi there,

 for a while.
 
It works pretty well until two days ago.
 
The detail of the error message is the following. I am wondering if my dev board is bad or something like that.
 
Any idea what happened and how to fix it?
 
Thank you very much
 
--Kenny
 
ERROR: Could not connect to target.
  SEGGER J-Link GDB Server V7.94b Command Line Version
  JLinkARM.dll V7.94b (DLL compiled Dec 13 2023 16:59:37)
  Command line: -SettingsFile "/source/nfc_pn7642/application/Debug/nfc_pn7642 JLink Debug SettingsFile.jlink" -nosilent -swoport 2337 -select USB=505001876 -jlinkscriptfile /Documents/MCUXpressoIDE_11.9.0_2144/workspace/.mcuxpressoide_packages_support/PN7642_support/Script/pnev7642fama.jlinkscript -telnetport 2338 -singlerun -endian little -noir -speed 4000 -port 2339 -vd -device PN7642 -if SWD -halt -reportuseraction
  -----GDB Server start settings-----
  GDBInit file:                  none
  GDB Server Listening port:     2339
  SWO raw output listening port: 2337
  Terminal I/O port:             2338
  Accept remote connection:      yes
  Generate logfile:              off
  Verify download:               on
  Init regs on start:            off
  Silent mode:                   off
  Single run mode:               on
  Target connection timeout:     0 ms
  ------J-Link related settings------
  J-Link Host interface:         USB
  J-Link script:                 /Documents/MCUXpressoIDE_11.9.0_2144/workspace/.mcuxpressoide_packages_support/PN7642_support/Script/pnev7642fama.jlinkscript
  J-Link settings file:          "/source/nfc_pn7642/application/Debug/nfc_pn7642 JLink Debug SettingsFile.jlink"
  ------Target related settings------
  Target device:                 PN7642
  Target device parameters:      none
  Target interface:              SWD
  Target interface speed:        4000kHz
  Target endian:                 little
  Connecting to J-Link...
  J-Link is connected.
  Device "PN7642" selected.
  Firmware: J-Link Ultra V5 compiled Dec 13 2023 14:34:48
  Hardware: V5.00
  S/N: 505001876
  Feature(s): RDI, FlashBP, FlashDL, JFlash, GDB
  Checking target voltage...
  Target voltage: 3.32 V
  Listening on TCP/IP port 2339
  Connecting to target...
  Found SW-DP with ID 0x6BA02477
  DPIDR: 0x6BA02477
  CoreSight SoC-400 or earlier
  Scanning AP map to find all available APs
  AP[1]: Stopped AP scan as end of AP map seems to be reached
  AP[0]: AHB-AP (IDR: 0x84770001)
  Iterating through AP map to find AHB-AP to use
  AP[0]: Skipped. Could not read CPUID register
  Attach to CPU failed. Executing connect under reset.
  DPIDR: 0x6BA02477
  CoreSight SoC-400 or earlier
  Scanning AP map to find all available APs
  AP[1]: Stopped AP scan as end of AP map seems to be reached
  AP[0]: AHB-AP (IDR: 0x84770001)
  Iterating through AP map to find AHB-AP to use
  AP[0]: Skipped. Could not read CPUID register
  Could not find core in Coresight setup
  Found SW-DP with ID 0x6BA02477
  DPIDR: 0x6BA02477
  CoreSight SoC-400 or earlier
  Scanning AP map to find all available APs
  AP[1]: Stopped AP scan as end of AP map seems to be reached
  AP[0]: AHB-AP (IDR: 0x84770001)
  Iterating through AP map to find AHB-AP to use
  AP[0]: Skipped. Could not read CPUID register
  Attach to CPU failed. Executing connect under reset.
  DPIDR: 0x6BA02477
  CoreSight SoC-400 or earlier
  Scanning AP map to find all available APs
  AP[1]: Stopped AP scan as end of AP map seems to be reached
  AP[0]: AHB-AP (IDR: 0x84770001)
  Iterating through AP map to find AHB-AP to use
  AP[0]: Skipped. Could not read CPUID register
  Could not find core in Coresight setup

  ERROR: Could not connect to target.
Re: PN7642 jlink error

OK. Here is what I did to solve the issue.

- After board operates in Mass-Storage mode

- Delete the CRP_00.BIN(180KB)

- Then copy one of the .bin application fw to the drive.

- Then my J-link works again.

Thanks Kelly for the hints.

--Kenny

Re: PN7642 jlink error

OK. I think I found the documentation for Mass-storage mode to update the firmware.

https://www.nxp.com/docs/en/application-note/AN13134.pdf page 54.

However, I have no idea which file I should put.

[kenny@MBP PN7642_FW_v02.02]$ ls -l
total 1840
-rw-r--r--@ 1 kenny staff 207995 Oct 10 2023 NXP_SLDA.pdf
-rw-r--r--@ 1 kenny staff 115 Oct 6 2023 PN7642_Default_AESChipKey.txt
-rw-r--r--@ 1 kenny staff 5702 Oct 6 2023 PN7642_Default_App_RSAKey.pem
-rw-r--r--@ 1 kenny staff 55036 Dec 15 2022 PN7642_SecureFW_SCR.pdf
-rw-r--r--@ 1 kenny staff 40114 Oct 9 2023 PN7642_v02.F2.esfwu
-rw-r--r--@ 1 kenny staff 1770 Oct 10 2023 ReadMe.txt
-rw-r--r--@ 1 kenny staff 306336 Oct 9 2023 phDnldNfc_UpdateSeq_v02.02.c
-rw-r--r--@ 1 kenny staff 256876 Oct 9 2023 phDnldNfc_UpdateSeq_v02.F2.c
-rw-r--r--@ 1 kenny staff 47842 Oct 9 2023 pn7642_v02.02.esfwu
-rw-r--r--@ 1 kenny staff 232 Oct 6 2023 version.txt

I assume that should be a bin file format.

Here is the screenshot when board operates in Mass-storage mode.

asknxp_0-1715174151097.png




--Kenny

Re: PN7642 jlink error

Hi Kelly,

I believe I am using FW02.02. OK. I will try to update the firmware again. Do you have a quick reference for using Mass-storge mode to update the firmware?

Thanks.

--Kenny

Re: PN7642 jlink error

Hello @asknxp 

What is your FW version? Or can you enter Mass-storage mode and update the firmware to the latest version (FW02.02)and try again.

BR

kelly

标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 10:25 PM
更新人: