1860663_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1860663_en-US

1860663_en-US

imxrt1176 freertos linkerscript file problem

I am trying to debug my project with freertos. However, I could not debug it. After some digging,

I found that project.ld (linker file) does not include the below line. (blue marked line).

This below SS belongs to app which can be debug.

burhanhagi_0-1715095904705.png


However, in my project, linker script file is as below;

burhanhagi_1-1715096025586.png

There must be a line between marked two lines in blue.

Since this linker script file is located in  "Debug folder", it is deleted when I add the required command manually. Therefore I need that  code line. How can I add it in order for linkerscript add automatically?


Re: imxrt1176 freertos linkerscript file problem

@diego_charles  thank you very much

Re: imxrt1176 freertos linkerscript file problem

Hi @burhanhagi 

To avoid your linker script modifications getting overwriten you can un-tick the Manage linker script 

diego_charles_0-1715105312087.png

But this may not be the best solution since MCUXpresso will not longer update the linker script. 

This section should be included to new project  when the FreeRTOS OS is selected. See the below snapshot. 

diego_charles_1-1715106201196.png


diego_charles_0-1715106165203.png

Now, if you do not want to create a new project, you can use the Manage SDK options and select FreeRTOS.

diego_charles_3-1715106469120.png

diego_charles_4-1715106510015.png

After clicking OK the below window will pop-up. Please consider that the IDE will ask if you wish to update your current SDK drivers, depending on your project and its configuration this could, in the worst scenario some clonficts, just be aware of that. 


diego_charles_2-1715106452511.png

After buiding, you should see the missing section. 




I really hope this could help you 

Diego



タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 03:17 PM
更新者: