Hi,
when I create a new project with S32K344, compilation work
but if i configure a pin and update code,compilation failed
directory platform install is \NXP\S32\S32DS\software\PlatformSDK_S32XX_4_0_0\RTD\Base_TS_T40D11M40I0R0
but message is
D:/NXP/S32/S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M40I0R0/include/OsIf_Internal.h:45:10: fatal error: OsIf_Cfg.h: No such file or directory
when I compile
i reinstall package and my problem has resolved
Have you installed multiple RTD versions under one S32 DS?
Installing different RTD versions under the same S32 DS will cause some similar errors.
This is somewhat similar to what I told you before.
If possible, you can uninstall the IDE and reinstall it and Please remember to delete all files in the installation directory.
but i don't have peripheral , components view, and Osif configuration so i can't add this file
when i click on the peripherals tools, it display "The peripheral tool is enabled but it does not support the selected processor"
Because you have not generated the OS. Press the generate button in peripheral>>OS>>general. And update the project
i reinstalled package with S32 extensions and updates
RTD S32K3_S32M27X 4.0.0.202404020208 com.nxp.RTD.S32K3_S32M27X.root.feature.feature.group NXP Semiconductors, Inc.
RTD S32K3XX 4.0.0.202404020208 com.nxp.RTD.S32K3XX.root.feature.feature.group NXP Semiconductors, Inc.
S32K3xx development package 3.5.8.202311290134 com.nxp.s32ds.s32k3.dev.feature.feature.group NXP
S32 Design Studio for S32 Platform 3.5.11.202403280939 com.nxp.s32ds.platform.ide.feature.feature.group NXP
FREERTOS S32K3_S32M27X 4.0.0.202312180411 com.nxp.FREERTOS.S32K3_S32M27X.root.4.0.0.feature.feature.group NXP Semiconductors, Inc.
i create a project with a guide_started_s32k_3xx and compilation is OK
but i tried to configure a pin and i have a error
D:/NXP/S32DS.3.5/S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M40I0R0/include/OsIf_Internal.h:45:10: fatal error: OsIf_Cfg.h: No such file or directory
i don't understand why this file is not inside my project
when i use the "manager SDK component"
i selected "OS" package and i have files related in OS in my project
Does this project come from S32DS?
Have you installed multiple RTD versions under one S32 DS?
Installing different RTD versions under the same S32 DS will cause some similar errors.
Please be sure to install a separate S32 DS for each RTD versions.
Have you properly started from demo project for S32K344? please check
thanks,
to have more information, here the message when i select peripheral
my configuration is S32K344, why is not compatible ?
Please try opening a sample project from S32 DS and test if such problem still exists.
If yes, it may be an issue with the RTD installation
If not, check your project and compare the difference between the two projects.
It seems you have not generated the OS code. Please check in the Peripheral setup, in OS>Generate you find Generate Configuration button. Press it and then update the code