Hi,
I have flashed imx8mmevk with 6.6.3-lts kernel. I have use case to enable dpdk and validate on it.
As per DPDK documentation I tried to use --vdev=net_enetfec and it also loaded pmd it seems as error presented was from enet_uio.c in dpdk driver code.
While from the error it seems device path of uio in /sys/class/uio and /dev/uio is missing.
I looked for if enet_uio is enabled from config in /proc path and it show the config option for driver was enabled. but I could n't found the .ko file for uio and enet_uio.
Any suggestion here to enable and run dpdk.
Thanks,
Vikas
Thanks it worked.
Please use imx8mm-evk-dpdk.dtb