Hello everyone!
I'm currently working on the S32K344EVB-Q257 board and i am trying to explore some of its safety features and, while installing the S32 Design Studio v3.5 along with Real-Time Drivers, i came across Safety Peripheral Drivers (which include drivers for FCCU, EIM, ERM, and STCU). I installed all of these, but when i create a project and go to the Peripherals Tab to add these latter drivers, nothing about FCCU, EIM, ERM or STCU shows up. Is this a bug/problem of this version of the drivers or am i missing something? Below i included an image of the Drivers that appear when i try to add them to the project.
2024-05-02_10h54_02.png
Thanks for any help in advance!
Note: RTD Version: R21-11 4.0.0 P04
SPD Version: RTM 1.0.4
Best regards,
JRodrigues
Hello Vane,
After your reply i have been able to see the drivers in Config Tools.
Thank you for your help!
Best Regards,
JRodrigues
Hi @JRodrigues
Make sure that you correctly install the S32K3_SAF_1.0.4_EVAL_DS_updatesite.zip, if this was correctly installed you should be able to find the package in Installation Details as shown in the following image.
VaneB_0-1714679747556.png
Also, if the package was correctly installed you should be able to visualize a tab named S32_SAF in Config Tools where you can add the Safety Peripheral Drivers to your project.
VaneB_1-1714679790989.png
B.R.
VaneB