1856632_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1856632_en-US

1856632_en-US

S32K312 default example, why is the core clock 160MHz, not 120MHz ?

Hi ,

Our project uses s32k312 as the MCU.

RTD2.0.0

The core_clk is 120MHz in reference manual.

Nitrogen8212_1-1714382594266.png

when I open the default example, I discover the CORE_CLK is 160MHz, not 120MHz, why?

Nitrogen8212_0-1714382511058.png


Re: S32K312 default example, why is the core clock 160MHz, not 120MHz ?

OK, thank you very much.

Re: S32K312 default example, why is the core clock 160MHz, not 120MHz ?

Hi @Nitrogen8212,

In S32K312, CORE_CLK=160Mhz can still run, but it is not recommended, as there will be unknown risks. You can see this was changed in later versions of the RTD packages of S32DS 3.5 RTD3.0.0 & 4.0.0:

Julin_AragnM_1-1714413300709.png

Best regards,
Julián

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 03:36 PM
Updated by: