1856054_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1856054_en-US

1856054_en-US

SENSOR SELECTION MPXV5010

IN MPXV5010 IF P1 > P2 OUTPUT GOES FROM 0.2 TO 5VOLT , I NEED SENSOR EXACT OPPOSITE WITH SAME RATING MEANS P1< P2 THEN OUT GOES 0.2 TO 4.5VOLT IS IT POOSIBLE OR SUGGEST PACKAGE OF THE MPXV5010G6U WHICH WILL HAVE ACCES TO USE THE p2 PORT FOR VACCUME INPUT , please suggest sensor with have vacuume pressure port is with port attched 

Re: SENSOR SELECTION MPXV5010

thanks

Re: SENSOR SELECTION MPXV5010

Hello Kumod,

Exact to -10 kPa is not available.

BR, Tomas

Re: SENSOR SELECTION MPXV5010

exact o to -10kpa is available or not

Re: SENSOR SELECTION MPXV5010

Hello Kumod,

We can offer the following vacuum pressure sensors:

https://www.nxp.com/products/sensors/pressure-sensors/vacuum-sensors-50-to-115-kpa:VACUUM_-50-115KPA

The closest one would be either the MPXV7007DP or MPXV7025DP.

BR, Tomas

标记 (1)
无评分
版本历史
最后更新:
‎02-04-2026 09:23 AM
更新人: