Hello,
I'm trying to use PWM to control the intensity of the red LED on the S32K358, so I try to follow section 4 of this tutorial:
Like the tutorial 4.3, I set the Emios to enable via Mcu -> McuModuleConfiguraion ->McuModeSettingConf - >McuPeripheral
But my EmoisCommon settings are greyed out:
I'm not sure what to do now. Without the EmoisCommon config, it's giving me the error on PwmemiosBufsRef
Can anyone help me out? Thanks.
For being able to configure Emios settings inside Mcl, you should have the following check enabled inside the Mcl General Configuration tab, as illustrated below.
Hope this helps,
Irina