1854816_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1854816_en-US

1854816_en-US

Where can I download the s32k sdk module documentation?

When I started to use S32K3, I wanted to know the meaning of each module of SDK and macl, but I could not find the relevant documents.

SDK: SW32K3_RTD_4.4_2.0.0_DS

MCAL: SW32K3_RTD4.4_R21-11_3.0.0_D2303

EB tresos 29.0EB tresos 29.0EB tresos 29.0s32ds for s32 platform 3.5s32ds for s32 platform 3.5s32ds for s32 platform 3.5

Re: Where can I download the s32k sdk module documentation?

Hi @harryoceana 

The User Manual for all S32K3 Drivers can be found in the file created when the.exe is installed, for example, C:\NXP\SW32K3_RTD_R21-11_3.0.0_P07\eclipse\plugins\Adc_TS_T40D34M30I0R0\doc, or if you are using S32DS can be found at C:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K3_2022_03\SW32K3_RTD_4_4_2_0_0_D2203\Adc_TS_T40D34M20I0R0\doc

Additionally, we have an application note about Migration Guide SDK/MCAL to Real-Time Drivers. Check it, it might be useful for you. 

AN13435: SDK/MCAL to Real-Time Drivers.


B.R.

VaneB

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 03:43 PM
Updated by: