Hi
I am facing an issue with S32D, when I am trying to debug,it gives me this error:
I have reinstalled the S32D and Pemiro drivers,but still have the same issue.
Hi @Ayaz
Please create a blank "S32DS Application Project" and see if you get the same error. Also, try with an example code.
Additionally, can you please try the following?
This power-up procedure manages that SBC starts with the disabled watchdog. Four orange LEDs indicate active 12, 5, 3.3, and 1.5 V power supply domains.
Hi
This is not the first time, and I figured that the issue was from the evaluation board (S32k344 Q172), when I am switching to (S32k344 T172). I did not have this issue anymore, do you have any idea, how to fix this?
Hi @Ayaz
What project are you flashing to the target? Is it one of the example projects or a custom one? Is this the first time you ever tried or did it work previously and now fail? Are you using custom boards? Or is it an NXP board?
B.R.
VaneB