1852242_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1852242_en-US

1852242_en-US

i.MX 6UltraLite MAC address

Hi,

I have a board with i.MX 6UltraLite (MCIMX6G2CVM05AB) and a LAN connection by the PHY transceiver KSZ8081RNBIA-TR of Microchip.

I see the MAC address changes every time a reset the board. So I need some explanation:

- Is the i.MX 6UltraLite who generates the MAC address?

- Is there a way to have a univoque value for the MAC address?

Best regards,

Andrea

Communication & Control(I3C | I2C | SPI | FlexCAN | Ethernet | FlexIO)Re: i.MX 6UltraLite MAC address

Hello @AndreaB-17 


If you want an unique MAC address you can burn the fuses:

21B_C620  -> Value of OTP Bank4 Word2 (MAC Address) (OCOTP_MAC0)


21B_C630 -> Value of OTP Bank4 Word3 (MAC Address) (OCOTP_MAC1)


You can do it in U-boot with fuse prog.


Best regards.


Salas.

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 03:49 PM
Updated by: