1848635_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1848635_en-US

1848635_en-US

S32DS S32K1xx_flash.ld Startup_code. s

I am using the S32DS S32K144 chip and I would like to use my own S32K1xx_flash.ld file and Startup_code. s file instead of being automatically generated by the system.

Every time I clean up the project, these files will be deleted, which is inconvenient. Is there any way to do this.

ld.pngld.png

Yesterday I found out that the ld file seems to have been modified here, but Startup.Code. s still doesn't know what to do

Re: S32DS S32K1xx_flash.ld Startup_code. s

Hi, 

sorry for delay. Clean the project don't delete any source code. Source code can be replaced for example if you generate code for SDK. 

You can add your own startup code into src folder and exclude Project_Settings/Startup folder from build: 

jiri_kral_1-1715854926636.pngjiri_kral_1-1715854926636.png




Re: S32DS S32K1xx_flash.ld Startup_code. s

Hi, 

sorry for delay. Clean the project don't delete any source code. Source code can be replaced for example if you generate code for SDK. 

You can add your own startup code into src folder and exclude Project_Settings/Startup folder from build: 

jiri_kral_1-1715854926636.pngjiri_kral_1-1715854926636.png




Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 04:06 PM
Updated by: