I have different groups using different versions of the RTDs depending on which project they're working on. Unfortunately, the RTDs are not backward compatible.
I have S32K3XX Real-Time Drivers AUTOSAR R21-11 Version 4.0.0 installed.
Another project was built with version 3.0.0. If I import the project, the configurator reports many errors and will not generate code.
When I tried to install version 3.0.0, S32DS says it cannot install it because a newer version is already installed.
What's the best way to support different projects that use different versions of the RTDs and what is the best way to figure out what version of platform tools needs to be installed to support them?
Hi @hns80,
Unfortunately, there is no current way to install multiple RTD packages in the same instance, as a workaround, you can install multiple instances for S32DS like:
c:\NXP\S32DS.3.5_RTD300\
c:\NXP\S32DS.3.5_RTD400\
and then install specific RTD to each instance.
Best regards,
Julián