We want to exercise the Suspend Mode on PN7462 EVK on the phExCcid SDK example. The EVK is connected to the Laptop through a micro USB cable. We configured the macro as PH_EXNFCCCID_USB_IF_USB_SUSPEND_RESUME_FTR 1 and run the code in debug mode.
I am getting prevention reason as E_HOSTCOMM_ONGOING though there is no ongoing communication with the Host. Why is there prevention? Or could you share a proven example of Suspend Mode?
PN7462
Thanks
@KaiLi Thanks for pointing to the right document.
The PH_EXCCID_USB_IF_USB_REMOTE_WAKEUP_FTR macro also needs to be set as 1.
Hello @Bhavin-Dhulkotiya
It's recommended that you refer to the below example and document to debug your device.
Example project: SW368334\ExamplesPN7462AU\phExNFCCcid
Document: https://www.nxp.com/docs/en/user-guide/UM10915.pdf
BR
kelly