1841047_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1841047_en-US

1841047_en-US

TWR-K70F120M + TWR-PROTO-ND without TWR-ELEV possible?

I have a TWR-K70F120M, can I use the prototype board (TWR-PROTO-ND) without the elevators (TWR-ELEV)?

I was wanting to see if I could add some simple passive components by connecting one side of the prototype board to one side of the K70 board.

Re: TWR-K70F120M + TWR-PROTO-ND without TWR-ELEV possible?

Hi,

This is the schematics of TWR-PROTO:

https://www.nxp.com.cn/downloads/en/schematics/SCH-26187.pdf

The TWR-ELEV board can connect the primary side signals of TWR-K70F120M to the TWR-PROTO board.

If you do not want to use TWR-ELEV, pls refer to  the schematics of TWR-K70F120M and check if you can connect the signals of TWR-K70F120M to the TWR-PROTO board, in other words, if the signals on TWR-K70F120M board you want to connect to are connected to a connector on the TWR-K70F120M board so that you can use flying cable to connect them. so it is case by case.

Hope it can help you

BR

XiangJun Rong


 


Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 04:21 PM
Updated by: