1839610_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1839610_en-US

1839610_en-US

Breakpoint FreeRtos debugging

Hello , 
I can 't have an enabled breakpoint , also FreeRtos tasks (threads) I can't see them however. I create 4 tasks.

AchrafOukheir_0-1712080194441.png

Maybe it's not well configured. I am based on the Freertos s32k344 example.

maybe my debugger doesnt support FreeRtos, my debugger is :

AchrafOukheir_0-1712082323905.png






Re: Breakpoint FreeRtos debugging

Hi,

I am using S32 DS V3.4 , using Free RTOS with 2 task. When i try to debug, breakpoint are hitting at very first time, but after triggering Resume option, breakpoints are not hitting. 


Anyone please give me some suggestion to resolve this error.

Re: Breakpoint FreeRtos debuggingThank you. If the breakpoints are resolved, the FreeRTOS debugging features will work.Re: Breakpoint FreeRtos debugging

Hi @AchrafOukheir 

According to the shared images, looks like you have selected the Skip All Breakpoints. This command marks all breakpoints in the current view as skipped. Breakpoints marked as skipped will not suspend execution. 

VaneB_0-1712266326956.png


B.R.

VaneB

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 04:23 PM
Updated by: