Please post questions directly in the forum.
For new users many old versions of S32DS and patch packages may no longer be available for download. So the solution has changed.
I installed it and it still doesn't work.
Hi.
This "opens the configuration .mex Error in: The current tool version does not support the processor version " This is usually caused by the S32DS Update n or S32K3 Development Package not having the version mentioned in the RTD Release Note installed.
Please install in S32DS v3.4.
| 3.4.3_D2112 | S32 Design Studio for S32 Platform v.3.4 Update 3 with support for S32K3 devices |
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct " button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
The S32K5 has not yet been officially released, and there are no public links on the NXP website to download software packages such as RTD and Development Pack. These types of problems are usually caused by these software packages not being installed correctly.
Please contact your company's FAE for assistance. Our online technical support will only be available after the official release of this type of NPI product.
Best Regards,
Robin