1832649_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1832649_en-US

1832649_en-US

Example S32K324 Bootloader to Application Jump DS3.5 RTD300

*******************************************************************************

 The purpose of this demo application is to present a usage of the
Bootloader Jump to Application.


 ------------------------------------------------------------------------------
* Test HW: S32K3X4EVB-Q172
* MCU: S32K324
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************

Jump is decided based on the boot_header, size we use to jump to the RESET handler:--

Dinesh_Guleria_0-1711002521870.pngDinesh_Guleria_1-1711002609276.png

Cortex M-7 Interrupt vector table, RESET handler is 4 byte offset from starting of vector table :--

Dinesh_Guleria_2-1711002629763.png
Dinesh_Guleria_3-1711002630207.png


How to burn elf file of both application & bootloader code :--

Dinesh_Guleria_4-1711002684831.png

Bootloader Linker file used :--

Dinesh_Guleria_5-1711002777353.png

Application Linker file used :--

This linker file has provision to distribute RAM to both the cores

Dinesh_Guleria_6-1711002777358.png

Application & bootloader both commented this, as CORE-1 should be started in CORE-0 main() function if required  :--

Dinesh_Guleria_7-1711002777393.png

System.c file this changed (as in RTD-3.0.0 bug in startup file because of which HARDfault occurs in startup process for S32K324) :--

Dinesh_Guleria_8-1711002777414.png
Tags (1)
No ratings
Version history
Last update:
‎11-19-2025 03:46 AM
Updated by: