1830452_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1830452_en-US

1830452_en-US

Kinetis (../45/47/43;MCX W71/72/70) & MCX W23 Power Profile Tools (including Localization)

This page is dedicated to the Kinetis (KW35/KW38/KW45/KW47) and MCX Wx (MCX W71/72 & MCX W23) Power Profile Tools.

It will help you to estimate the power consumption in your application (Automotive, IIoT, Trackers/Tags and Continuous Glucose Monitoring [CGM]) and evaluate the battery life time of your solution.

This page contains 4 market segments which provides dedicated power profile tool on standalone product or full system application for:

   1. Automotive

Kinetis (KW3x/4x) Power Profile Tools for Automotive - NXP Community

    1. Bluetooth LE for the KW35/36 products in standalone.
    2. Bluetooth LE for the KW37/38/39 products in standalone.
    3. Bluetooth LE for the KW45/KW47 products in standalone.
    4. SmartFob application (BLE/KW45; UWB Ranger4; SE; motion sensor) 
    5. SmartFob application (BLE/KW47; UWB Ranger5; SE; motion sensor) 

   2. IIoT

Kinetis MCX Wxx (MCX W71/72 & MCX W23) Power Profile Tools for IIoT - NXP Community

    1. Bluetooth LE for the MCX W71/MCX W72 product in standalone.
    2. Bluetooth LE for the MCX W23 product in standalone.
    3. 802.15.4 Matter ICD SIT & LIT and ZED for the MCX W71 & W72 product in standalone (IIoT).
    4. Aliro Doorlock application

   3. Localisation application (CCC CS) for Automotive & IIoT

Kinetis MCX Wxx (KW47 & MCX W72) Power Profile Tools for Bluetooth Localization - NXP Community


   4. New tools coming:

    1. Zephyr Zboss
    2. Zephyr BLE

Please, find this important link to build a PCB using a KW45/MCX W71 or KW47/MCX W72 and all concerning the radio performances and radio certification (CE/FCC/IC):

The best way to build a PCB using a KW45 (car acce... - NXP Community


For Power and Low Power Application Notes please see product pages. Here are some direct links for your convenience:

MCXW71 - Power Management Hardware

KW45/K32W148 - Power Management Hardware


A different experience: One Connectivity Power Profiling tool

It includes all the Connectivity power profiling tools in one.

Kinetis (KW3x/4x, MCX W7x and MCX W23) One Connectivity Power Profile Tool - NXP Community

Note: This tool is quite slow but very interesting to compare Kinetis products.

Product: K32W0Product: K32W1Product: KW 34|35|36Product: KW 37|38|39Product: KW41Z |31Z | 21ZProduct: QN9080|SIPProduct: QN9090|30Re: Kinetis (KW35/38/KW45 & K32W1/MCX W71) Power Profile Tools (including Localization)

Hi Everett,

The password is in place to avoid changes or competitor benchmarks in too much details.

Sorry for the inconvenient but it can't be.

Re: Kinetis (KW35/38/KW45 & K32W1/MCX W71) Power Profile Tools (including Localization)

Hi  christophe_menard,

@christophe_menard  Could you provide the password of Sheet protection, thanks very much.

EverettRao_0-1729134009121.pngEverettRao_0-1729134009121.pngEverettRao_0-1729134009121.png


Re: Kinetis (../45/47/43;MCX W71/72/70) & MCX W23 Power Profile Tools (including Localization)

Hello ,

We would like to work with OneConnectivityPowerProfilingtool_SDK_26_03.zip but a trojan is detected.

How to do to use thtis tool.

Thank you for the support

Re: Kinetis (../45/47/43;MCX W71/72/70) & MCX W23 Power Profile Tools (including Localization)

Hi @pierre_demeyer 

I opened a ticket to our IT to verify this.

I will keep you informed soon.

Re: Kinetis (../45/47/43;MCX W71/72/70) & MCX W23 Power Profile Tools (including Localization)

Hi @pierre_demeyer 

After IT verification, no Trojan virus was detection using Crowstrike or Defender softwares.


タグ(1)
評価なし
バージョン履歴
最終更新日:
3 週間前
更新者: