1828242_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1828242_en-US

1828242_en-US

Is S32K3 TCPIP RTM 1.0.1HF1 based on S32K3 RTD RTM2.0.0 or based on S32K3 RTD RTM2.0.1

I tested S32K3-T-BOX using S32K3_T_BOX_LWIP_for_S32K3.zip.I install S32K3 RTD RTM2.0.0 and FreeRTOS2.0.0,but i can not install TCPIP RTM 1.0.1HF1(It prompts me to install S32K3 RTD RTM2.0.1).

However, the code supported by NXP WEB is depended onS32K3 RTD RTM2.0.0.

I can not find TCPIP RTM 1.0.1 without HF1 on nxp web,only TCPIP RTM 1.0.1HF1.

Can you give me a code based on S32K3 RTD RTM2.0.1 or a TCPIP RTM 1.0.1 without HF1?

Re: Is S32K3 TCPIP RTM 1.0.1HF1 based on S32K3 RTD RTM2.0.0 or based on S32K3 RTD RTM2.0.1

Hi @xMaryAES,

Please enter a support case through Support Ticket

Re: Is S32K3 TCPIP RTM 1.0.1HF1 based on S32K3 RTD RTM2.0.0 or based on S32K3 RTD RTM2.0.1

Hi @Julián_AragónM ,

Could you please share with me too the TCP/IP RTM 1.0.1 without HF1 or guide me to where I can find it?

S32K3-T-BOX 

Thank you! Regards.


Re: Is S32K3 TCPIP RTM 1.0.1HF1 based on S32K3 RTD RTM2.0.0 or based on S32K3 RTD RTM2.0.1

Hi @Julián_AragónM ,

Could you please share with me the TCP/IP RTM 1.0.1 without HF1 compatible with S32K3 RTD RTM2.0.0?

Regards,

T1AES

Re: Is S32K3 TCPIP RTM 1.0.1HF1 based on S32K3 RTD RTM2.0.0 or based on S32K3 RTD RTM2.0.1

Could you send the  S32K3 TCPIP RTM 1.0.1 without hf1 to me ? thank you.

Re: Is S32K3 TCPIP RTM 1.0.1HF1 based on S32K3 RTD RTM2.0.0 or based on S32K3 RTD RTM2.0.1

Hi @SCoder41,

I'm not sure about the visibility in Flexera, but I have sent you a private message with the UpdateSite for TCP/IP RTM 1.0.1 without HF1.

Best regards,
Julián

标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 09:10 AM
更新人: