1805940_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1805940_en-US

1805940_en-US

MMA8452QR1

Good morning Team,

MMA8452QR1 is this obsolete component? If yes, any alternative options like-for-like available?

Re: MMA8452QR1

2.4Mu at www.rocelec.com


Re: MMA8452QR1

MMA8452QR1 has sufficient stock, it is not recommended that you replace it, 1$

Re: MMA8452QR1

Rochester Electronics has partnered with NXP Motion Sensor team to offer EOL products. We have acquired extensive authorized NXP inventory on MMA8452QR1/MMA8453Q1/MMA8451Q1. Please visit www.rocelec.com to view our extensive NXP Accelerometer inventory. 

Re: MMA8452QR1

Do you have something available that meets or exceeds the "sensitivity change versus temperature" and "zero-g level change versus temperature" of the MMA8452QR1?

Re: MMA8452QR1

Hello abialevich1,

I hope all is great with you. Thank you for using the NXP communities.

You are correct, the MMA8452Q device is obsolete. Unfortunately, we do not have a direct replacement. I mean, pin-to-pin compatible.

In this case, I would like to recommend the following series from our accelerometer portfolio:

FXLS8967AF - ±2g/±4g/±8g/±16g, Low Power 12-bit Digital Accelerometer

I hope this information helps.

Regards,

David

Tags (1)
No ratings
Version history
Last update:
‎02-04-2026 05:22 AM
Updated by: