1789908_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1789908_en-US

1789908_en-US

Example S32K312 PIT BTCU parallel ADC FIFO DMA DS3.5 RTD300

This example for S32K312 is based on this, example on S32K344 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-PIT-BTCU-parallel-ADC-FIFO-DMA-DS3-...


*******************************************************************************

 The purpose of this demo application is to present a usage of the
 ADC_SAR and BCTU IP Driver for the S32K3xx MCU.

 The example uses the PIT0 trigger to trigger BCTU conversion list to
 perform parallel conversions on ADC0/ADC1. Three ADC channels
 are selected to be converted on each ADC:
 ADC0: S8 , P0, S8
 ADC1: S10, S13, S17
 Converted results from BCTU FIFO are moved by DMA into result array.

 ADC channel S10 is connected to board's potentiometer.


 ------------------------------------------------------------------------------
* Test HW: S32K3X4EVB-Q172
* MCU: S32K312
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE Micro
* Target: internal_FLASH
********************************************************************************
Set PIT Freeze Enable :---

Dinesh_Guleria_0-1707202447324.pngDinesh_Guleria_0-1707202447324.png


BCTU will be do the parallel conversion for channel mentioned in BCTU list :--

Dinesh_Guleria_3-1707204479195.pngDinesh_Guleria_3-1707204479195.png

 

Dinesh_Guleria_1-1707202600904.pngDinesh_Guleria_1-1707202600904.png
"NEW DATA DMA enable mask" :--
controls These bit field in MCR register

Dinesh_Guleria_0-1707203759290.pngDinesh_Guleria_0-1707203759290.png

"ADC target mask" :--

It controls "ADC_SEL " bit field in "Trigger Configuration (TRGCFG_0 - TRGCFG_71)"

for single conversions you can enable only one instance
so the possible values for target mask:
1 (0b001) ADC0
2 (0b010) ADC1
3 (0b100) ADC2|

for list of conversions we can enable also parallel con version
for example
3 (0b011) parallel conversion of ADC0 and ADC1


The trigger is configured as a list of parallel conversions ADC0, ADC1 in “Adc Target Mask”.
List of ADC channels is defined in “BCTU List Items” while order is given by the “Adc Target Mask”: BctuListItems_0 is ADC0, BctuListItems_1 is ADC1 etc.


Dinesh_Guleria_3-1707204011310.pngDinesh_Guleria_3-1707204011310.png



Dinesh_Guleria_4-1707204043898.pngDinesh_Guleria_4-1707204043898.png
Dinesh_Guleria_2-1707203974137.pngDinesh_Guleria_2-1707203974137.png



Result :--
I connected VDD from board on adc_0_p0 (PTD1 : J412-1)  and adc_1_p2 (PTE0 J412-13).
Also POT value on S10 of ADC-1 & ADC-0-VREFH value coming correct & STABLE.

Dinesh_Guleria_1-1707330412160.pngDinesh_Guleria_1-1707330412160.png

Dinesh_Guleria_0-1707330375235.pngDinesh_Guleria_0-1707330375235.png




=========================Using  FIFO-2 =================

Dinesh_Guleria_0-1732514437470.pngDinesh_Guleria_0-1732514437470.png



FIFO-2 Trigger & LIST Index :--

Dinesh_Guleria_1-1732514506589.pngDinesh_Guleria_1-1732514506589.png



Dinesh_Guleria_2-1732514539640.pngDinesh_Guleria_2-1732514539640.png


ADC channel conversion :--

Dinesh_Guleria_3-1732514707504.pngDinesh_Guleria_3-1732514707504.png





Tags (1)
No ratings
Version history
Last update:
‎11-19-2025 03:48 AM
Updated by: