The pressure sensor MPXV7002 has following temperature ranges:
operating: TA +10...+60°C
Do may cause permanent damage if operating at -10°C...+9°C? [yes or no]
I can accept in my project that the error will increase outside of the compensated temperature range (+10...+60°C), but I cannot accept that the sensor will be permanent damaged, as stated in the datasheet (Table 4. Maximum Ratings, note [1]).
Thank you for your help.
Dear Andrea,
yes, you can use the MPXV7002DP outside of the compensated temperature range (TA +10...+60°C), from -30°C to 100°C without damage. But as you mentioned the error is increased outside of the compensated area and we cannot guarantee how much.
With Best Regards,
Jozef