1628182_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1628182_en-US

1628182_en-US

Code Warrior 10.5.1 for PA - Install New Software not working

I have Code Warrior for PA 10.5.1 installed and I am trying to add QCVS (for RCW work). The installation was done as a clean new install.

When I try to use Install New Software I get errors.

Please help.

Also, links to any offline install packages do not work for me (they send me back to the NXP Code Warrior main page).

FYI - if I try to navigate to any of the update locations in a web browser I get 'Page Not Found'.

The generated error is:

Some sites could not be found. See the error log for more detail. Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.pkt_win/content.xml. Remote host closed connection during handshake Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.buildtools_win/content.xml. Remote host closed connection during handshake Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.qcvs_win/content.xml. Remote host closed connection during handshake Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.updatesite_win/content.xml. Remote host closed connection during handshake

Re: Code Warrior 10.5.1 for PA - Install New Software not working

Still I was not able to get the tool

Getting error as below

image.pngimage.png

Re: Code Warrior 10.5.1 for PA - Install New Software not working

I was able to get this working by modifying where the installation new software tool gets the new software, since it's still pointing to the old freescale.com address. If you go to help -> install new software... then click on the "available Software Sites" then update some of the locations to nxp from freescale, including the QCVS you should be able to get the tool. 

petes1_3-1758000269386.pngpetes1_3-1758000269386.png


petes1_2-1758000206672.pngpetes1_2-1758000206672.png


petes1_1-1758000123163.pngpetes1_1-1758000123163.png



Re: Code Warrior 10.5.1 for PA - Install New Software not workingHi, Can you send the QCVS offline installation packages to me

Thank you
Re: Code Warrior 10.5.1 for PA - Install New Software not working

I've used the link

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=6529687&dkey=9017647

But it would not work for you.


You should:

0. log in to nxp

1. Open ticket support

2. Get a link from support

3. Support->Click on ticker -> Click on download, approve commitment and then goto next protal:

i.e. the link something as above.

it will be valid for a few days.


Re: Code Warrior 10.5.1 for PA - Install New Software not working

How can I get a copy of this, those sites are still down.... 

Re: Code Warrior 10.5.1 for PA - Install New Software not working

Can you send the offline install file to me, Thanks a lot!

Re: Code Warrior 10.5.1 for PA - Install New Software not working

Can you send the offline install file to me, Thanks a lot! Also

Re: Code Warrior 10.5.1 for PA - Install New Software not workingI have already got one, Thanks a lot!Re: Code Warrior 10.5.1 for PA - Install New Software not working

Can you send the offline install file to me, Thanks a lot!

Re: Code Warrior 10.5.1 for PA - Install New Software not working

I actually found the QCVS for PA 4.5 here and successfully added to codewarior-10.5.1.

Attached a screenshot of the location. It may useful for others.

Re: Code Warrior 10.5.1 for PA - Install New Software not working

Hi,

Thanks for the offline install file. I have this installed and working now with Code Warrior 10.5.1.

Note I needed to de-select the option "Contact all update sites during install to find required software", else the install would fail with an error.

Thanks again

Re: Code Warrior 10.5.1 for PA - Install New Software not working

I have transcended QCVS offline installation packages for CodeWarrior for Power Architectures Rev 4.5 to you, please pay attention to your email box to download it.

After downloading QCVS for PA 4.5, please open CodeWarrior for PA 10.5.1 IDE, then install QCVS package from "Help->Install New Software->Add->Archive"

Re: Code Warrior 10.5.1 for PA - Install New Software not working

I've got a bit further with this.

The Install New Software not working was because CodeWarrior installer still sets the download site as the old 'freescale.com'. I have edited and replaced with 'cache.nxp.com'. This information was very difficult to find! The QCVS installer now runs but generates MD5 hash errors (see attached). This also happens when running any of the update sites (build tools, eclipse, etc.). It also does the same in other versions of CodeWarrior (we also have v10.3). How do I sort this out?

Re: Code Warrior 10.5.1 for PA - Install New Software not working

Hi, Thanks for the answer. QoriQ Configuration and Validation Suite doesn't appear in my NXP software list. Also does not appear under the Code Warrior list. See screenshots attached. I am currently using an evaluation copy of Code Warrior 10.5.1. We have a licensed copy of Code Warrior 10.3 but have not upgraded yet. The online docs for Code Warrior says QCVS is free (unlicensed) so I wanted to try out and start looking at PBL/RCW configuration for our QoriQ T-series based boards. How do I get QCVS in my Code Warrior? Thanks again.


Re: Code Warrior 10.5.1 for PA - Install New Software not working

You could download QCVS for Power Architectures Rev 4.5 from NXP public Web site.

Please login "www.nxp.com", then download the installation file from "My NXP Account->Software Licensing and Support->View accounts->NXP Software->QorIQ Configuration and Validation Enablement Suite-> 4.5 QCVS offline installation packages for CodeWarrior for Power Architectures Rev 4.5.

After downloading QCVS for PA 4.5, please open CodeWarrior for PA 10.5.1 IDE, then install QCVS package from "Help->Install New Software->Add->Archive".

Then reopen CodeWarrior IDE, create a QCVS PBL project from "File->New->QorIQ Configuration Project", please enter "Project name" and select the processor to be used, click Next. Then in "Toolset selection" panel, please select "PBL - Preboot Loader RCW configuration"

Re: Code Warrior 10.5.1 for PA - Install New Software not working

Hi, Can you send the QCVS offline installation packages to me.

Thank you!

Re: Code Warrior 10.5.1 for PA - Install New Software not workinghello,could you please send one to meRe: Code Warrior 10.5.1 for PA - Install New Software not workingHi,

Open CodeWarrior for PA 10.5.1 IDE and add the below repository in "Help->Install New Software->Add" to install QCVS

http://cache.nxp.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.qcvs_win
Tags (1)
No ratings
Version history
Last update:
‎07-23-2026 03:28 AM
Updated by: