1429076_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1429076_en-US

1429076_en-US

About rt1052 sdk2.11.0 Example usb_device_msc_disk

rt1052 development board connected to an 8G sd card, now there is such a need: sd card front 4G for rt1052 normal read and write, the back of the 4G want to virtualize into a USB flash drive through the usb for computer use. The operation is as follows.

1. sd card fatfs has been correctly partitioned as follows:

944706426_0-1647416415404.png944706426_1-1647416425150.png


2, run usb_device_msc_disk example, the results of the normal recognition of the two partitions;

944706426_3-1647416597854.png



3, but I only want to be recognized by the PC sd card first partition, so try to modify, as follows

944706426_4-1647416701206.png

The result is that only the first partition is recognized, and it works fine, but I'm not sure if this is the right way to change it, please ask the NXP technician to help me, thank you very much!

944706426_2-1647416518201.png




回复: 关于rt1052 sdk2.11.0 例子usb_device_msc_diskand the actual USB flash drive is formatted (the files on it have been erased)回复: 关于rt1052 sdk2.11.0 例子usb_device_msc_diskHello, I would like to ask your side through the computer on the USB flash drive format (quick format), can normal formatting success, my side through the pc to format USB flash drive, has been prompted: windows can not complete the formatting.Re: 关于rt1052 sdk2.11.0 例子usb_device_msc_disk

Hi @944706426.

Should work, only tell the OP half the space.


Regards.

Jing

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 08:58 AM
更新者: