1405288_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1405288_en-US

1405288_en-US

LPC55S69 Getting nowhere with SPI - DMA - Linked or Ping-Pong transfers

This has dragged on for far too long now...

I've been through the examples for single SPI/DMA transfers and these work.

I've been through the examples for DMA/Linked memory transfers and these work.

But none cover my requirement and try s I might I can't get one to fit.

I need a free running SPI TX/RX using DMA with either linked configurations or just ping-pong to start.

Surely there must be someone on here that's achieved this already, who'd be willing to share some knowledge?

The best I've managed so far is a set of linked configurations for SPI_DMA, which execute just once (despite the last linking back to the first) and then stop.

The worse is a single 8-bit transfer for linked 16-bit transfers.

I'm running out of ideas and pretty sure I'm now trying things that have already failed.

Anybody..?


GeneralLPC55xxPeripheralsRe: LPC55S69 Getting nowhere with SPI - DMA - Linked or Ping-Pong transfers

I know this is an old post, but anyway... the problem is related with the width of your tx transfer. To configure the fifo must be 32 bits (16 data + 16 cfg) or you have all the configuration bit in the spi that are zeroes, with the problems you are experiencing.

--gra


Re: LPC55S69 Getting nowhere with SPI - DMA - Linked or Ping-Pong transfers

Hi @IanMcCarthy 


I would like to apologize for the delay. We are experimenting an anormal volume of questions these days. I really thank you for your patience.


Regarding your question, once you do a single manual start (run on debug session), all the code has to run indefinitely, and SCK from SPI has to generate more than 2 pulses (continuosly until you press stop). I would like to ask for you which example from our SDK you are using for LPC55S69? What changes did you make to the code? So I can reproduce your code on my board and see what is going on.


Thank you so much for your help. Please let me know if you have more questions.


Best Regards.
Pablo Avalos.

Re: LPC55S69 Getting nowhere with SPI - DMA - Linked or Ping-Pong transfers

Third attempt to post an update...

I need to continuously receive data from a slave SPI device at a fixed rate (manually triggering won't meet the requirements).

The code below shows where I'm currently at, but this just generates 2 SPI clock pluses and that's it.

I'm assuming once SPI is configured I can configure a linked set of DMA descriptors and after a single manual start, this will run indefinately, or am I mistaken?

If someone would be willing to help out, it'd be much appreciated.

    srcClock_Hz = EXAMPLE_SPI_MASTER_CLK_FREQ;

    SPI_MasterGetDefaultConfig(&masterConfig);
    masterConfig.sselNum = (spi_ssel_t)EXAMPLE_SPI_SSEL;
    masterConfig.sselPol = (spi_spol_t)EXAMPLE_MASTER_SPI_SPOL;
    masterConfig.dataWidth = kSPI_Data8Bits;

    masterConfig.baudRate_Bps = 8000;

    SPI_MasterInit(EXAMPLE_SPI_MASTER, &masterConfig, srcClock_Hz);
    DMA_Init(EXAMPLE_DMA);

    // Enable channels
    DMA_EnableChannel(EXAMPLE_DMA, EXAMPLE_SPI_MASTER_TX_CHANNEL);
    DMA_EnableChannel(EXAMPLE_DMA, EXAMPLE_SPI_MASTER_RX_CHANNEL);

    // Set channel priorities
    DMA_SetChannelPriority(EXAMPLE_DMA, EXAMPLE_SPI_MASTER_TX_CHANNEL, kDMA_ChannelPriority3);
    DMA_SetChannelPriority(EXAMPLE_DMA, EXAMPLE_SPI_MASTER_RX_CHANNEL, kDMA_ChannelPriority2);

    // Create channel handles
    DMA_CreateHandle(&masterTxHandle, EXAMPLE_DMA, EXAMPLE_SPI_MASTER_TX_CHANNEL);
    DMA_CreateHandle(&masterRxHandle, EXAMPLE_DMA, EXAMPLE_SPI_MASTER_RX_CHANNEL);

    // Set channel callbacks
    DMA_SetCallback(&masterTxHandle, TxCallback, NULL);
    DMA_SetCallback(&masterRxHandle, RxCallback, NULL);
    DMA_SetupDescriptor(
    		&dmaTxDescriptors[0],
				DMA_CHANNEL_XFER(true, false, true, false, 1, 0, 0, 1),
				&masterTxData,
				(void *)&SPI7->FIFOWR,
				&dmaTxDescriptors[1]);

    DMA_SetupDescriptor(
    		&dmaTxDescriptors[1],
				DMA_CHANNEL_XFER(true, false, true, false, 1, 0, 0, 1),
				&masterTxData,
				(void *)&SPI7->FIFOWR,
				&dmaTxDescriptors[2]);

    DMA_SetupDescriptor(
    		&dmaTxDescriptors[2],
				DMA_CHANNEL_XFER(true, false, true, false, 1, 0, 0, 1),
				&masterTxData,
				(void *)&SPI7->FIFOWR,
				&dmaTxDescriptors[0]);


    DMA_PrepareChannelTransfer(&dmaChannelConfig,
    		&masterTxData,
				(void *)&SPI7->FIFOWR,
				DMA_CHANNEL_XFER(true, false, true, false, 1, 0, 0, 1),
				kDMA_MemoryToPeripheral,
				NULL,
				// &dmaChannelTrigger,
				&dmaTxDescriptors[0]
    );

    DMA_SubmitChannelTransfer(&masterTxHandle, &dmaChannelConfig);

    DMA_StartTransfer(&masterTxHandle);

Re: LPC55S69 Getting nowhere with SPI - DMA - Linked or Ping-Pong transfers

I haven't totally understood your answer, could you please further explain? Why not keeping the uint8_t width of the transfer?



I have also noticed that the 3rd and 4th input parameters of the function DMA_SetupDescriptor() are in the incorrect place.

Additionally, shouldn't each descriptor destination address re-direct the data to another memory position, instead of all of them pointing to &masterTxData ?

Tags (1)
No ratings
Version history
Last update:
3 weeks ago
Updated by: