1367532_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1367532_en-US

1367532_en-US

MCU Flash Loader Reference Manual

Chapter 1 Introduction

The MCU Flash Loader is a configurable flash programming utility that operates through serial communications on the
MCU . It enables quick and easy programming
of MCUs throughout the product lifecycle, including application development and final product manufacturing . The MCU Flashloader will be available in highly configurable binary or full source code form. Host-side command
line and GUI tools can be used to communicate with the Flashloader. Users can use the host tools to upload and
/or Or download the application code.

Chapter 2 Flash Loader Protocol

This section describes the general protocol for data packet
transfer
between the host and the MCU flash loader. The description includes data packet transfers of different transactions, such as commands without a data phase and commands with an incoming or outgoing data phase.

Chapter 3 Flash Loader Packet Types

The MCU Flash Loader device works in slave mode. All data communications are initiated by the host, which can be a PC
host or an embedded host. The
MCU Flash Loader device is the target machine that receives commands or data packets. All data communications between the host and the
target machine are in packetized form.

Chapter 4 MCU Flash Loader API

All MCU Flash Loader command APIs follow
the command packet format wrapped by framing packets as described in the previous sections.

Chapter 5 Supported Peripherals

This subsection describes the peripherals supported by the MCU Flash Loader.

Chapter 6 External Memory Support

This subsection describes
the external memory devices supported by the
MCU Flashloader. To properly use an external memory device, you must enable the device using the corresponding configuration file. The Flashloader cannot access an external memory device that is not enabled. The MCU Flashloader uses the memory identifier to enable a specific external memory device as shown below.

Chapter 7 Security Utilities

The MCU flash loader supports certain security utilities for easy generation of security related blocks. Note that
the flash loader itself must first be signed in order to properly enable the security utilities.

IndustrialTechnologies
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎01-05-2026 12:36 PM
更新者: