1365251_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1365251_en-US

1365251_en-US

MCU-LINK not working

Hi,

I am trying to use an MCU-LINK on a new PC (Windows 10 laptop) unfortunately without much success!

I installed mcuxpresso, and when I plug the MCU-LINK into a USB port it makes the usual noise like it is enumerating, but mcuxpresso cannot see the probe and in Windows device manager, there is a yellow warning triangle next to the "USB composite device" that appears with a message in device status that says "This device cannot start (Code 10). Insufficient system resources exist to complete the API"

I also tried manually downloading the MCU-LINK driver installer for Windows 10 from the NXP website, but still no success.

Any pointers please? This is a relatively new laptop which I would not expect to be short on resources for this.

Many thanks

-Nick


Re: MCU-LINK not working

Hello,

I found myself with the exact same problem.

I just managed to solve it, so hopefully it can be usefull. I did the following:

Going to C:\nxp\LinkServer_26.6.137\MCU-LINK_installer\scripts , click in "program_CMSIS", then follow the instructions on the command pannel (i.e., Short Jumper J3 of the MCU-link -> Connect via USB the MCU-link -> press space bar).

(Otherwise you can try write "CMSIS" or look for "Program MCU-Link CMSIS-DAP" in the search bar of Windows to find directly the file).

After perfoming this, the device was properly recognised without warnings by the computer in Device Manager and i could successfully debug my board.


Not sure if related, or if it helped to work (maybe not required), but before performing that firmware update of the mcu-link i did:

1- Did "Windows Security" -> "App & browser control" -> Smart App Control settings -> off.

2- I re-installed the LinkServer installer, which you can find in "LinkServer for Microcontrollers" on nxp website.

Also, after doing firmware update:

1- open mcuxpresso IDE with "run as administrator", and then on the project Explorer, i opened the project folder, and in the bottom i deleted the folder "(*project_name*)_ LinkServer Debug.launch" before debugging the code.


This is the way that it worked for me. Hope someone finds it useful as well.

Best, Kans.

Re: MCU-LINK not working

hi, im also using mcu-link, its working fine, when its connected directly to the laptop port, but when im using a usb hub, and connecting the mcu -link through that usb hub, the debbugging is not working, its throws an error, how can i overcome this?, im only having one port in my laptop, so its neccessary to use via an hub


Re: MCU-LINK not working

I can think of two other alternatives:

One is making sure your Antivirus is not detecting the MCU-LINK as a threat, and disabling it for good measure.

The second is trying with a different computer. If the problem persists with a different machine, then we have reasons to believe that the problem could be MCU-LINK related. Otherwise, I believe the problem is most likely related to the OS or the cable.

I hope this helps.

Re: MCU-LINK not working

thanks @EdwinHz 

Yes, we downloaded the drivers from that location.

We are not using a USB hub, this is a direct connection.

Will try a different USB cable, but this seems unlikely.

Any other suggestions please? Thanks!

 

Re: MCU-LINK not working

Hi @nickwallis,

The drivers that you installed manually were from the “MCU-Link installer for Windows 10” software found at the bottom of the MCU-Link Debug Probe website? If not, I would recommend reinstalling the drivers using this installer.

Check the connection to your MCU-LINK. If it’s connected to a USB hub try connecting it directly to the machine. Also try using a different USB cable.


Regards,

Edwin.

Tags (1)
No ratings
Version history
Last update:
a week ago
Updated by: