1346363_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1346363_en-US

1346363_en-US

imx8mp hdmi 4k display

I am using imx8mp evk development board, linux kernel version is linux-imx-5.10.9. using HDMI interface, I found that the default output is 1080p@60, how can I modify the kernel to make the HDMI output 4K.

Re: imx8mp hdmi 4k 显示Hello, I've encountered this problem on my side as well, is it convenient to know how you ended up solving this problem?Re: imx8mp hdmi 4k 显示

Uh, thanks.

The crux of the matter is that we are a medical device company, previously the UI was developed in QT, the platform was your imx6 imx7, and now we are using your 8 for our high end product line. All the previous code was based on fb, it would be costly to switch to drm now ............ Never mind, I'll do some more research and see if I can modify that part of your source code to create different numbers of fbx based on the number of monitors plugged in.

Re: imx8mp hdmi 4k 显示

Desktop systems don't use fb0 and use drm nodes, even if fb0 is available, we don't recommend it, the mainstream is the drm framework.

Re: imx8mp hdmi 4k 显示

I did not move your kernel on the fb0 generation of the source code, now with your bsp inside the exact same, your source code inside the drm framework is to use the last generated a fb0, on this one, regardless of inserting a few screen is also on this one fb

Re: imx8mp hdmi 4k 显示

That is to say lvds and hdmi are plugged in the case, although the two resolutions are not the same, but the kernel application buffer is in accordance with the resolution of the lvds, hdmi and lvds display are also used when the buffer, so that led to the hdmi display abnormal now? Then it's hard to figure out ..........

Re: imx8mp hdmi 4k 显示

I thought hdmi switched resolutions adaptively.

-->Based on the DRM API you can realize the buffer allocation under different CRTC, but if you write fb0 directly, that's how you get this display mismatch problem. The buffer you allocate in the application layer must be for a certain screen, such as LVDS resolution size buffer, then you write in, the underlying driver just throws this buffer directly into the lcd controller, the driver layer is very stupid not adaptive. You throw in how much resolution buffer, he will be displayed so large.

Re: imx8mp hdmi 4k 显示

We are trying to realize dual screen simultaneous display, qt writes image data to fb0, and we want the image data in fb0 to be displayed on 1200*768 lvds and 1920*1080 hdmi at the same time. Do you think this can't be done? Right now the qt side is using a form of eglfs, for simultaneous display it has to be something like eglfs-kms that operates directly on the cardx node generated by the drm to work?

Re: imx8mp hdmi 4k 显示

My current lvds screen is 1200*768 and hdmi supports resolutions up to 1920*1080. So you mean that for the lvds and hdmi to display properly, the hdmi resolution also has to be manually set to something like 1200*768 or a similar resolution to work? I thought the hdmi would adaptively switch resolutions, I see from the hdmi monitor settings that the screen display resolution is now 1920*1080, and the image displayed on the hdmi is only a piece in the upper left corner, and the size is similar to the size of the lvds!

Re: imx8mp hdmi 4k 显示

It's been measured and can automatically recognize 4K.

lvds and hdmi share the same fb0 node generated by the drm framework

--" Isn't this only one resolution? With your shared fb0, are the LVDS and HDMI screen resolutions the same?

Re: imx8mp hdmi 4k 显示

Is there a solution? I also have a problem now, lvds and hdmi share the same fb0 node generated by the same drm framework, after both lvds and hdmi are connected, the size of the image displayed by the hdmi is the same size as the lvds, it doesn't spread over the whole hdmi display, what's going on?

Re: imx8mp hdmi 4k 显示

I can see the same thing. I'll give you the solution later.

Re: imx8mp hdmi 4k 显示

I burned demo images of L5.10.35_2.0.0 and tried them on 2K and 4K screens, and they still only display 1080p.

Use modetest to check HDMI maxes out at 1920x1080@60 and doesn't have 4k resolution

Re: imx8mp hdmi 4k 显示

HMDI display resolution is adaptive, you try L5.10.35_2.0.0 demo images

标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 06:38 PM
更新人: