1329183_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1329183_en-US

1329183_en-US

MC33AR6000 Blind Zone truth table

Blind Zone is designed a current gap when excitation start raising at very beginning.  This feature is designed for a mechanical coupling delay time when engine start.

Customer can fuse the blind zone as initiation, or config/inhibit blind zone by LIN command.

Customer can refer to the attachment truth table find the blind zone result.


LIN have higher priority.

when BZI(OTP)=BZI(LIN)=1, BZ output=0%

For other cases:

1. LIN mode: BZ=BZ(LIN)

2. Defult mode: BZ=BZ(OTP)

BZI(OTP) BZ(OTP) BZI(LIN) BZ(LIN) BZ output
Version A & B
0 X X 0 3%
0 X X 1 12%
1 X 0 0 3%
1 X 0 1 12%
1 X 1 0 0%
1 X 1 1 0%
version C
X X   00 0%
X X   01 3,125%
X X   10 6,25%
X X   11 12,50%
version E
X X   0 3%
X X   1 6%
No LIN
X 00 X X 0%
X 01 X X 3,250%
X 10 X X 6,00%
X 11 X X 12,00%

Alternator Regulator
Tags (1)
No ratings
Version history
Last update:
‎11-19-2025 11:52 AM
Updated by: