1283624_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1283624_en-US

1283624_en-US

Release Announcement - GUI Guider v1.1

The latest version of GUI Guider was recently released by NXP. If you are unfamiliar with GUI Guider it is a graphical development tool for creating UIs on supported NXP microcontrollers. The tool allows you to create a UI, test the UI along with various levels of events all within a simulation environment, and then deploy the UI application directly to the NXP development board or generate the code for use in MCUXpresso IDE. GUI Guider is designed specifically for use with LVGL, an open-source graphics library, that is available within the MCUXpresso SDK.

 

This release of GUI Guider features:

  • New Development Tool capabilities
    • Menu shortcut and keyboard control
    • New states: FOCUSED, EDITED, DISABLED
    • Frame rate customization
    • Screen transition configuration
    • Parent / children widgets
    • Callback function setting for animation image
    • VGLite enablement
    • Header path auto-config

  • New or improved Widgets
    • BMP and SVG assets
    • 3D animation for PNG

  • HW Acceleration capabilities
    • Initial support for VGLite on RT1170 and RT595

  • New Device Target Supported

New release of GUI Guider v1.1, the user-friendly graphical user interface development tool from NXP that enables the rapid development of high quality displays with the open-source LVGL graphics library.

标记 (1)
无评分
版本历史
最后更新:
‎11-19-2025 03:21 PM
更新人: