1280075_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1280075_en-US

1280075_en-US

Can qemu emulate i.MX 8M Plus ?

We do not have i.MX 8M Plus board, so I'd like to ask if qemu can emulate i.MX 8M Plus?

I'd like to run qemu Linux based on i.MX 8M Plus.

Can the qemu Linux run applications compiled by XTENSA, like the SOF project?

Thank anyone who can give any information.

Re: Can qemu emulate i.MX 8M Plus ?

I solved the issue. QEMU’s i.MX8MP emulation already creates its own USB controllers (DWC3/XHCI). I was adding a separate EHCI USB controller using the command -device usb-ehci,id=ehci, and these two controllers were working independently. The device I attached to the EHCI controller couldn’t communicate with the i.MX8MP’s actual USB bus. I removed the EHCI controller and instead used the board’s built-in USB controller, and that allowed me to successfully connect the camera to the board.

Here’s the working command:


 
sudo /home/arif/src/qemu/build/qemu-system-aarch64 \ -M imx8mp-evk -smp 4 -m 3G -display none -serial null -serial stdio \ -kernel /home/arif/imx-qemu/buildroot-2024.11.1/output/images/Image \ -dtb /home/arif/imx-qemu/buildroot-2024.11.1/output/images/imx8mp-evk.dtb \ -append "root=/dev/mmcblk2p2" \ -drive file=/home/arif/imx-qemu/buildroot-2024.11.1/output/images/sdcard.img,if=sd,bus=2,format=raw,id=mmcblk2 \ -device usb-host,bus=usb-bus.0,port=1,vendorid=0x04f2,productid=0xb729 \ -monitor telnet:127.0.0.1:4444,server,nowait
 

Re: Can qemu emulate i.MX 8M Plus ?Hello,
I am emulating the i.MX8MP board in QEMU and trying to connect my laptop’s built-in camera to the board using USB passthrough.
I used the following command:

sudo /home/arif/src/qemu/build/qemu-system-aarch64 \
-M imx8mp-evk -smp 4 -m 3G -display none -serial null -serial stdio \
-kernel /home/arif/imx-qemu/buildroot-2024.11.1/output/images/Image \
-dtb /home/arif/imx-qemu/buildroot-2024.11.1/output/images/imx8mp-evk.dtb \
-append "root=/dev/mmcblk2p2" \
-drive file=/home/arif/imx-qemu/buildroot-2024.11.1/output/images/sdcard.img,if=sd,bus=2,format=raw,id=mmcblk2 \
-usb -device usb-ehci,id=ehci -device usb-host,hostbus=1,hostaddr=3


When I checked the camera on the host, I saw the “device not found” error — meaning QEMU successfully captured the device —
but when I listed connected USB devices inside QEMU, the camera was not visible at all.

Do you have any idea what I might be doing wrong? I would really appreciate your help.
Re: Can qemu emulate i.MX 8M Plus ?

Finally,I run the qemu command:

qemu-system-aarch64 \
    -machine virt  \
    -cpu cortex-a53 \
    -smp 4 \
    -m 2G \
    -kernel ./Image \
    -drive file=imx-image-full-imx8mpevk.qcow2,if=none,id=drive0,format=qcow2 \
    -device virtio-blk-pci,drive=drive0 \
    -append "root=/dev/vda2 rootwait rw console=ttyAMA0,115200" \
    -netdev user,id=eth0 \
    -device virtio-net-device,netdev=eth0 \
    -device virtio-gpu-pci \
-nographic
the virtual machine can setup successfully.
Re: Can qemu emulate i.MX 8M Plus ?

I run the qemu setup command:

qemu-system-aarch64 \
-machine imx8mp-evk \
-cpu cortex-a53 \
-m 2G \
-smp 4 \
-kernel ./imx-image-full-imx8mpevk/boot/Image \
-drive file=imx-image-full-imx8mpevk.qcow2,format=qcow2,id=disk,if=none \
-append "root=/dev/vda console=ttyAMA0"

the system can't be loaded successfully.Can you help me check the command, the argument -kernel is right?

Re: Can qemu emulate i.MX 8M Plus ?

no, Xtensa is not supported by qemu.


Re: Can qemu emulate i.MX 8M Plus ?

Thank you for the reply.

Could  I ask for another question about qemu + i.MX 8M Plus?

I'd like to know qemu + i.MX 8M Plus supports emulating xtensa dsp core?

How to run a xtensa application under qemu + i.MX 8M Plus?

Re: Can qemu emulate i.MX 8M Plus ?

Hello mm2021,

The qemu-system-aarch64 binary supports all the 32-bit CPUs and boards, in the same way that qemu-system-x86_64 lets you run a 32-bit x86 CPU guest, which is why the list is so long and full of 32-bit boards. You cannot just try to use a 32-bit board with a -cpu cortex-a53, since is 64 bits.


Regards


タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 06:32 PM
更新者: