1272092_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1272092_en-US

1272092_en-US

How to use the HCI_bb on Kinetis family products and get access to the DTM mode

This article is presenting 2 parts:

   Part1: How to flash the HCI_bb binary into the Kinetis product (here is the example of the KW38).

   Part 2: Perform RF measurements using the R&S CMW270 


2 attached files:

   - bci_black_box.bin (zip file)

   - mbed_WinSerial.exe (zip file)



Part1: How to flash the HCI_bb binary into the Kinetis product (here is the example of the KW38).

The HCI_bb application example is on the SDK folder below:

christophe_menard_0-1620204656370.png



Plug the FRDM-KW38 board on your PC using the USB cable.

The FRDM-KW38 board will be seeing as a hard disk. Disk in this example.

Select the hci_black_box_frdmkw38.bin file and drag and drop this file to the FRDM-KW38 (D:)

christophe_menard_1-1620204656478.png


The KW38 is flashed when 100% is reached.

christophe_menard_2-1620204656494.png

The FRDM-KW38 board is ready to be used with the DTM mode.


Part 2: Perform RF measurements using the R&S CMW270 

The FRDM-KW38 board could be connected to the R&S CMW270 using the USB cable.

The hci_bb set the KW38 in DTM mode.

The CMW270 could communicate by sending DTM commands.

Note: You need to install the mbedWinSerial driver (attached in this article) in the CMW270 to detect the FRDM-KW38 board.

Re: How to use the HCI_bb on Kinetis family products and get access to the DTM mode

I am trying to doing this DTM test on KW36(specific application hardware, not a development board) ,can you please help or share the entire process as well as firmware & list of tools required to perform this test?

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-23-2026 03:28 AM
更新者: