1202244_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1202244_en-US

1202244_en-US

Adding Openjdk support to zeus yocto layer

Environment: openjdk-8 with L5.4.24-2.1.0 and GCC-9

1. Clone meta-java with dedicated branch name:

git clone git://git.yoctoproject.org/meta-java -b zeus

2. Update .bb file for compile error in meta-java:

diff --git a/recipes-core/icedtea/icedtea7-native.inc b/recipes-core/icedtea/icedtea7-native.inc
index 8d0dc71..153a604 100644
--- a/recipes-core/icedtea/icedtea7-native.inc
+++ b/recipes-core/icedtea/icedtea7-native.inc
@@ -26,7 +26,7 @@ CXXFLAGS_append = " -fno-tree-dse"
CXX_append = " -std=gnu++98"

# WORKAROUND: ignore errors from new compilers
-CFLAGS_append = " -Wno-error=stringop-overflow -Wno-error=return-type"
+CFLAGS_append = " -Wno-error=stringop-overflow -Wno-error=return-type -Wno-error=format-overflow"

inherit native java autotools pkgconfig
inherit openjdk-build-helper

3. Add meta-java layer into bblayers.conf:

BBLAYERS += "${BSPDIR}/sources/meta-java"

4. Edit the conf/local.conf to add openjdk variables

# Possible provider: cacao-initial-native and jamvm-initial-native
PREFERRED_PROVIDER_virtual/java-initial-native = "cacao-initial-native"

# Possible provider: cacao-native and jamvm-native
PREFERRED_PROVIDER_virtual/java-native = "jamvm-native"

# Optional since there is only one provider for now
PREFERRED_PROVIDER_virtual/javac-native = "ecj-bootstrap-native"

PREFERRED_PROVIDER_java2-runtime = " openjdk-7-jre"
IMAGE_INSTALL_append = " openjdk-7-jdk "
diff --git a/recipes-core/openjdk/openjdk-8-common.inc b/recipes-core/openjdk/openjdk-8-common.inc
index d8b30b8..ed03d60 100644
--- a/recipes-core/openjdk/openjdk-8-common.inc
+++ b/recipes-core/openjdk/openjdk-8-common.inc
@@ -181,5 +181,5 @@ FLAGS_GCC9 = "-fno-lifetime-dse -fno-delete-null-pointer-checks"
BUILD_CFLAGS_append = " ${@openjdk_build_helper_get_build_cflags(d)}"
BUILD_CXXFLAGS_append = " ${@openjdk_build_helper_get_build_cflags(d)}"
# flags for -cross
-TARGET_CFLAGS_append = " ${@openjdk_build_helper_get_target_cflags(d)}"
+TARGET_CFLAGS_append = " ${@openjdk_build_helper_get_target_cflags(d)} -Wno-error=format-overflow"
TARGET_CXXFLAGS_append = " ${@openjdk_build_helper_get_target_cflags(d)}"
diff --git a/recipes-core/openjdk/openjdk-8-native.inc b/recipes-core/openjdk/openjdk-8-native.inc
index 321a43d..97ff03f 100644

5. Switch the host GCC to gcc-8 and g++-8:

sudo apt-get install gcc-8 g++-8
sudo update-alternatives --install /usr/bin/gcc gcc /usr/bin/gcc-8 --slave /usr/bin/g++ g++ /usr/bin/g++-8 --slave /usr/bin/gcov gcov /usr/bin/gcov-8 --slave /usr/bin/gcov-tool gcov-tool /usr/bin/gcov-tool-8 --slave /usr/bin/gcc-ar gcc-ar /usr/bin/gcc-ar-8 --slave /usr/bin/gcc-nm gcc-nm /usr/bin/gcc-nm-8 --slave /usr/bin/gcc-ranlib gcc-ranlib /usr/bin/gcc-ranlib-8
sudo update-alternatives --config gcc 

6. And change the conf/local.conf from openjdk-7 -> openjdk-8:

PREFERRED_PROVIDER_java2-runtime = " openjdk-8-jre"
IMAGE_INSTALL_append = " openjdk-8 " 
i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlus
标记 (1)
无评分
版本历史
最后更新:
‎11-19-2025 03:39 AM
更新人: