1190620_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1190620_en-US

1190620_en-US

Servomotor Arm

Overview


Within the industry it is necessary to use different types of motor control in which different ranges of precision or freedom of movement can be obtained. The servo motor control by pwm gives precise control by angles.


Required material


1x Kinetis K70 120 MHz Tower System Module

2x Tower System Elevator Module

5x Potentiometer

5x Servomotor

CodeWarrior

Video



Connections


bd pwm.pngbd pwm.png

Step-by-Step


1. Download the attached file2. Unzip it
3. Upload it to CodeWarrior

servo 2.pngservo 2.png

servo 3.pngservo 3.png

servo 4.pngservo 4.png
4. Compile it

servo 5.pngservo 5.png
5. Upload it to the TWR-K70 board
6. Make the connections in the diagram
7. Connect to Power Supply
8. The variation in the potentiometers will vary the position of each motor

Block DiagramsIndustrial
Tags (1)
No ratings
Version history
Last update:
‎11-20-2025 07:03 AM
Updated by: