1128458_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1128458_en-US

1128458_en-US

Using the FRDM-KL46 Board as a USB Mouse in KDS

USB Mouse in KDS

 

Description:

 

A project made in KDS using the accelerometer on a FRDM-MKL46Z256VLL4 board to control a USB mouse input.

A red LED will flash while not connected as a USB mouse, and green LED will flash when it is.

SW1 will right click.

SW3 will left click.

 

Sensitivity of the mouse can be changed by altering the HIDM1_Move command in main.c

 

Sections of code taken from:

- http://mcuoneclipse.com/2012/09/21/tutorial-accelerating-the-kl25z-freedom-board/

- http://mcuoneclipse.com/2013/08/01/using-the-frdm-kl25z-as-a-usb-mouse-device/

USB Mouse in KDS

 

Description:

 

A project made in KDS using the accelerometer on a FRDM-MKL46Z256VLL4 board to control a USB mouse input.

A red LED will flash while not connected as a USB mouse, and green LED will flash when it is.

SW1 will right click.

SW3 will left click.

 

Sensitivity of the mouse can be changed by altering the HIDM1_Move command in main.c

 

Sections of code taken from:

- http://mcuoneclipse.com/2012/09/21/tutorial-accelerating-the-kl25z-freedom-board/

- http://mcuoneclipse.com/2013/08/01/using-the-frdm-kl25z-as-a-usb-mouse-device/

General
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-19-2025 10:40 AM
更新者: