1125007_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1125007_en-US

1125007_en-US

QT5 Support for Qt3D

Before QT5 Qt3D was a separate project and was maintained separately.  Now it is offered along with other official plugins.

QT3D supports the addition of 3D elements. In order to install it this is needed:

Clone the git Qt3D repository

$ git clone git://gitorious.org/qt/qt3d.git

Using the Qmake that you already created when installing Qt5, this will setup the Makefile in order to cross compile the plugin.

$ qmake

$ make

$ sudo make install

Ready to play with Qt3D!

This is the HelloWorld of 3D,  teapot.bez  is a bezier curves file with the forms of the famous teapot.

import QtQuick 2.0

import Qt3D 1.0

Viewport{

   width: 640; height: 480

   Item3D{

   id: teapot

   mesh: Mesh { source: "teapot.bez" }

   effect: Effect {}

  }

}

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-19-2025 02:48 PM
更新者: