1122154_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1122154_en-US

1122154_en-US

Low power mode example code for MagniV S12ZVC device

The example code demonstrates MCU low power modes: STOP and WAIT. For detailed description see main.c file of the project.

* - tested on X-VLG-S12ZVC board

* - BUSCLK = 6.25MHz based on internal oscillator clock IRCCLK = 1MHz.The PLL set by default in PEI mode.

* - Reference documentation:

MC9S12ZVCRMV1.pdf (REV 1.9)

VLG-MC9S12ZVC-SCH.pdf (Document Number SCH-28038, SPF-28038)

GeneralRe: Low power mode example code for MagniV S12ZVC device

Hi Paolo,

It has been fixed, thank you,

BR, Daniel

Re: Low power mode example code for MagniV S12ZVC device

Hi guys,

where I can find the file EX-TIC-S12ZVC-STOPandWAITmode-CW106.zip?

The link seems to be broken "Not Found The item does not exist. It may have been deleted".

Regards

Re: Low power mode example code for MagniV S12ZVC device

Hi Daniel, 
Thank you very much for the effort.

Best regards,
Alexis

Re: Low power mode example code for MagniV S12ZVC device

Hi Alexis,

It has been updated.

Thanks.

Regards,

Daniel

Re: Low power mode example code for MagniV S12ZVC device

Hi guys,
It seems that the link is broken "Error 404 file not found".

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-19-2025 04:35 AM
更新者: