1121785_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1121785_en-US

1121785_en-US

i.MX6ULL_LPDDR2_Script_Aid

Following docs(English or Chinese version) are also can be referred as a hand on guide.

Freescale i.MX6 DRAM Port Application Guide-DDR3 

飞思卡尔i.MX6平台DRAM接口高阶应用指导-DDR3篇 

 

Please find i.Mx6DQSDL LPDDR2 Script Aid through below link.

i.Mx6DQSDL LPDDR2 Script Aid 

Please find i.Mx6DQSDL DDR3 Script Aid through below link.

i.MX6DQSDL DDR3 Script Aid 

Please find i.MX6SX DDR3 Script Aid through below link.

i.MX6SX DDR3 Script Aid 

Please find i.MX6SL LPDDR2 Script Aid through below link.

i.MX6SL LPDDR2 Script Aid 

Please find i.MX6UL DDR3 Script Aid through below link..

https://community.nxp.com/docs/DOC-329899 

Please find i.MX6UL LPDDR2 Script Aid through below link.

i.MX6UL_LPDDR2_Script_Aid 

Please find i.MX6ULL DDR3 Script Aid through below link.

i.MX6ULL_DDR3_Script_Aid 

Re: i.MX6ULL_LPDDR2_Script_Aid

Hi Jan,

Thanks for your question!

4 bank part are all smaller density (less than 512Mb), we do not validated it before.

So it is not included by the Aid.

If customer want to use that, they should develop by themself.

Re: i.MX6ULL_LPDDR2_Script_Aid

Hello LinWang‌,

I have noticed that changing the number of banks to 4 has no effect on MMDC0_MDMISC[DDR_4_BANK].

This is common to all Script Aids that I subsequently tried.

Could you please arrange for correction of the affected Script Aids?

Best Regards,

Jan

Tags (1)
No ratings
Version history
Last update:
‎11-19-2025 07:30 AM
Updated by: