1120180_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1120180_en-US

1120180_en-US

Patch to support Ethernet PHY KSZ8081 (Rev1) on i.MX6UL/i.MX6ULL EVK board

Overview

In latest i.MX6UL/i.MX6ULL EVK boards, Ethernet PHY chip is upgraded with new revsion ID (01) although the same part number KSZ8081RNBIA is used. The detailed change is as follows:

pastedImage_5.png

pastedImage_6.png

Mark on old Ethernet PHY chip (Silicon Revision ID is 0, Mark is A2):

            KSZ8081

            RNBIA

            1439A2T

            M147J18M02

Mark on new Ethernet PHY chip (Silicon Revision ID is 1, Mark is A3)

              KSZ8081

              RNBIA

              1602SA3T

               M159S28M23

                                 

Software Patch

Linux BSP requires to be updated to support this new Ethernet PHY because PHY setting is designed to be associated with silicon ID. See attached patch for the details (Please note: i.MX6ULL/i.MX6UL EVK shared the same board file.)

The formal patch is also included into the releases starting from L4.1.15_2.0.1. See http://git.freescale.com/git/cgit.cgi/imx/meta-fsl-bsp-release.git/tree/imx/meta-bsp/recipes-kernel/...

If ethernet doesn't function on your i.MX6UL/i.MX6ULL EVK board in kernel, please check whether Silicon Revion Mark is A3 on the board and then apply for attached file for the test.

i.MX6ULRe: Patch to support Ethernet PHY KSZ8081 (Rev1) on i.MX6UL/i.MX6ULL EVK board

Hi Llly,

On my imx6ul Evaluation board, Silicon Revision ID is 1, Mark is A3

I tried to patch but not successful.

root@imx6ulevk:~#
root@imx6ulevk:~# patch < /home/root/work/0001-ARM-imx-imx6ul-add-PHY-KSZ8081-new-silicon-revision-.patch 
patching file mach-imx6ul.c
patch: can't open 'mach-imx6ul.c': No such file or directory
root@imx6ulevk:~#

FYI, Linux version of my machine is 4.1.15-1.1.0+ga4d2a08 & machine model : freescale i.mx6 ultralight 14x14 Evk board

Please Help

Jaydeep

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-20-2025 06:31 AM
更新者: