1120001_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1120001_en-US

1120001_en-US

MCUXPresso IDE SWO Trace function

The MCUXpresso IDE SWO trace function is a special feature which enables user to observe variable update, interrupt entry/exit timing, interrupt event statistic, to print information in SWO ITM Console while the MCU is running. The MCUXpresso IDE SWO trace function is a supplement to the debugger of the MCUXpresso IDE. The main advantage is to display variable, print information, list interrupt entrying/exitting/returing while the MCU is running.

 The documentation describes the hardware connection to implement the SWO function, MCUXpresso configuration and source code to implement the function. 

标记 (1)
无评分
版本历史
最后更新:
‎11-20-2025 05:16 AM
更新人: