1118153_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1118153_en-US

1118153_en-US

MX8X_4.14.98_ga_kernel_V3-20190903_chn.pdf .i.mx8x内核代码定制文档<meta http-equiv="Content-Type" content="text/html; charset=utf-8" />

NXP BSP Core Customization........................................ 103
6.1 IO Pin Configuration and Pinctrl Driver................................... 103
6.2 Bringing up new boards .................................................. 118
6.3 Change the debug serial port: .................................................. 127
6.4 uSDHC device customization (eMMC flash, SDcard, SDIOcard)
133
6.5 LVDS LCD Driver Customization......................................... 142
6.6 GPIO_Key driver customization......................................... 145
6.7 GPIO_LED driver customization................................... 149
6.8 Fuse nvram driver.................................................. 152
6.9 SPI and SPI Slave Drivers................................... 153
6.10 USB 3.0 TypeC changed to USB 3.0 TypeA (unverified) ... 160
6.11 Automotive-Grade Ethernet Driver Customization........................ 160

i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlusLinuxRe: MX8X_4.14.98_ga_kernel_V3-20190903_chn.pdf .i.mx8x内核代码定制文档<meta http-equiv="Content-Type" content="text/html; charset=utf-8" />

updated to v3

Add nandflash
Support/DDR
Modification/i.MX8DX
support

Re: MX8X_4.14.98_ga_kernel_V3-20190903_chn.pdf .i.mx8x内核代码定制文档

firmware version should be: modify in next version

注意:也可以如下使用wget命令获得mx8qx-ahab-container.img

wget http://www.freescale.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.1.bin

chmod +x firmware-imx-8.1.bin  && ./ firmware-imx-8.1.bin --auto-accept

mx8qx-ahab-container.img位于firmware-imx-8.1/firmware/seco/mx8qx-ahab-container.img

标记 (1)
无评分
版本历史
最后更新:
‎01-05-2026 05:14 AM
更新人: