1117278_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1117278_en-US

1117278_en-US

Generate aligned HEX and S-record data output with GNU in KDS 3.2

Some customers have special requirements for the output data.  They need them to be aligned, especially when they are using the customized bootloader or Flash Programmer.  

 

However, the hex file generated in KDS3.2 is not aligned as the customer expected.

Below is extracted from the hex file generated in a KE06 project.  In this file, the data is not aligned at 16 bytes, and the size of each line is different.

154237_154237.pnghex_ori.png

 

The attached document shows generate aligned Hex and S-record file step by step.

General
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-19-2025 06:02 AM
更新者: