1116910_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1116910_en-US

1116910_en-US

G5 Engineering: IP Camera Solution based on the i.MX 6 Applications Processor

G5 Engineering demonstrates an IP camera solution based on i.MX6 apps processor at the FTF Americas 2014.

 


Features

  • Multiple IP cameras that are aggregated by one i.MX6 and then sent over an IP backhaul to a second i.MX 6 for integration into a single image
  • The images are brought out to the screen. No need to use Windows reducing virus instances
  • With a click of a button can change the display to 1x1 or 1x2 to 4x4 views

Featured NXP Products


Links

Industrial
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-19-2025 02:58 PM
更新者: