1116811_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1116811_en-US

1116811_en-US

P4080 USB Specific FAQs

If I don’t use the USB interface in the 4080, can I leave USBx_VDD_3P3 and USBx_VDD_1P0 pins not connected? In P4040 they are reserve with note do not connect. Can they be connected to 3.3V and 1.0V respectively?

USB_VDD_1P0 must be tied to 1V or the platform voltage (based on whatever the SOC core digital power supply is). USB_VDD_3P3 can be left floating.


If I don’t use USB, is it safe to leave USBx_IBIAS_REXT and USBx_VDD_1P8_DECAP unconnected?

If USB is not to be used at all, keep the following USB signals floating : USB1_IBIAS_REXT, USB2_IBIAS_REXT, USB1_VDD_1P8_DECAP and USB2_VDD_1P8_DECAP, USB1_VDD_3P3, USB2_VDD_3P3.


QorIQ P4 Devices
Tags (1)
No ratings
Version history
Last update:
‎11-19-2025 01:34 PM
Updated by: