1114944_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1114944_en-US

1114944_en-US

SDMA ap_to_ap Fixed Scripts (i.MX6DQ)

The attached patch applies to iMX6_Platform_SDK for i.MX6 Dual and Quad and brings 2 additional SDMA memory to memory scripts:

  • fixed destination address, increasing source address
  • fixed source address, increasing destination address.

With this patch, the new scripts are also integrated in the SDMA Test menu of the Platform SDK.

I created these scripts starting from the ROM script ap_to_ap. In order to dump the content of the SDMA ROM, I used mxc_printSDMAcontext function which is also included in the attached patch and can be invoked when needed.

i.MX6Duali.MX6QuadRe: SDMA ap_to_ap Fixed Scripts (i.MX6DQ)

Yes, it's in the ap domain.

Re: SDMA ap_to_ap Fixed Scripts (i.MX6DQ)

Thank you for the post.

Are these ap_to_ap_fixed RAM scripts capable of accessing the external EIM bus?

Example: Main RAM to  fixed address at  EIM bus

标记 (1)
无评分
版本历史
最后更新:
‎11-19-2025 03:09 PM
更新人: