1114557_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1114557_en-US

1114557_en-US

How to install KL03 SDK support in KDS 1.1.1 and KDS 2.0.0

This article describe procedure how to properly install support for KL03 derivative in KDS (Kinetis Design Studio) 1.1.1  (KDS 2.0.0) and also additional steps to update GCC compiler and debug firmware on the FRDM-KL03Z board.

KDS 1.1.1 (KDS 2.0.0) installation

If you don’t have KDS 1.1.1 (KDS 2.0.0), please get the installation package (for Windows and Linux) on Freescale website. Go to the page Kinetis Design Studio Integrated Development Environment (IDE), select the build and install it.

Kinetis SDK installation

The KL03Z derivative support is distributed as a service pack KSDK 1.0.0 for KL03Z.

Download the Freescale Kinetis SDK_1.0.0 for the FRDM-KL03Z Windows or Linux installer and install it.

After the KSDK 1.0.0 for KL03Z is installed you need also install the PEx service pack for KL03. In the KDS main menu select Help > Install new software… , click on Add.. button , click on Archive and select KL03Z-1.0.0-GA-SA-RC2-for-Eclipse.zip in the SDK subfolder (e.g. c:\Freescale\KSDK_1.0.0-KL03Z\tools\eclipse_update\KL03Z-1.0.0-GA-SA-RC2-for-Eclipse.zip):

pastedImage_7.png

Additional Steps

Next step is to install the updated GCC compiler. This is due to C standard library footprint issue in the GCC version that is distributed in KDS 1.1.1 (KDS 2.0.0). The KL03Z derivatives contain small amount of RAM memory and therefore this step is also strongly recommended.

Detailed instructions, how to update the GCC, are provided in the KSDK user guide located in the KSDK 1.0.0 for KL03Z installation folder in KSDK_1.0.0-KL03Z\doc\Kinetis SDK Freescale Freedom FRDM-KL03Z Platform User’s Guide.pdf – chapter Appendix B: Kinetis Design Studio environment variable fix and swap tool chain.

Please note that when you update the GCC you must change the linker flags for every new project with GCC to “-specs=nano.specs -specs=nosys.specs” as described in the document. (otherwise the default setting of linker flags will cause an error of GCC linker).

If you haven’t done that yet,  update firmware of the FRDM-KL03Z board to allow application flashing and debugging. It is described in the same document in the chapter Appendix C: OpenSDA J-Link firmware updated.

You can start creating a new application for the KL03 now. For example see Low power demo application on FRDM-KL03Z board.

Tags (1)
No ratings
Version history
Last update:
‎11-20-2025 03:44 AM
Updated by: