1112410_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1112410_en-US

1112410_en-US

HOWTO: S32 Design Studio Command Line Interface

Building Projects

There is already a significant amount of information already available on this topic. Please explore the external references listed below for detailed information.

External References

Building Projects with Eclipse

Build Several CDT C++ projects from command line

With the following command line, it is possible to build the project KEA128:

eclipsec -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data C:\Users\username\workspaceS32DS.ARM2.0 -build KEA128/Release

 

The project was located in workspace - C:\Users\username\workspaceS32DS.ARM2.0

Project Name is: KEA128

Build Configuration is: Release

Emitting Source Code

S32 Design Studio for Vision

Emitting the source code from the command line: There are 2 sections in the Reference Manual, one for each of the ISP and APEX2 Visual Graph Tools.

pastedImage_2.png

Processor Expert Software - S32 Design Studio

There is a section in the Processor Expert User Guide titled 'Command Line Interface'

pastedImage_9.png

Re: HOWTO: S32 Design Studio Command Line Interface

Hi @mikedoidge , 

I need support for S32D 3.4, S32DS.ARM2.0 No support for S32K3XX

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-19-2025 02:42 PM
更新者: